[S32DS 3.4] S32FlashTool for S32G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32DS 3.4] S32FlashTool for S32G

Jump to solution
1,491 Views
masatakayakashi
NXP Employee
NXP Employee

Hi,

A Debug tool vendor who is working for S32G is asking question about S32FlashTools.
They would like to perform Read/Write/Erase Flash by loading S32G2xxx.bin and MX25UW51245G.bin on SRAM via JTAG debugger. Is it possible? If yes, following questions are popped up.
Q1: Which address should they be stored in?
Q2: Which address is starting address?
Reading MX25UW51245G.bin, they found the address of FA_Init() and FA_ExecCmd(). Should they call FA_Init()? If so, the What value of argument "apParams" for FA_Init should be configured?
Q3: After calling FA_Init(), should they call FA_ExecCmd()?

Best Regards,
Masataka Yakashiro

0 Kudos
1 Solution
1,475 Views
mikedoidge
NXP Employee
NXP Employee

Hello @masatakayakashi,

We have a document regarding the command line use of the Flash Programmer within the S32 Debugger. It uses JTAG connection with S32 Debug Probe.

https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-wi...

Best Regards,

Mike

View solution in original post

0 Kudos
2 Replies
1,466 Views
masatakayakashi
NXP Employee
NXP Employee

Thanks, I will recommend to try S32Debugger.

BR

Masataka 

0 Kudos
1,476 Views
mikedoidge
NXP Employee
NXP Employee

Hello @masatakayakashi,

We have a document regarding the command line use of the Flash Programmer within the S32 Debugger. It uses JTAG connection with S32 Debug Probe.

https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-wi...

Best Regards,

Mike

0 Kudos