S32DS 2.2 ProcessorExpert.pe is disabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 2.2 ProcessorExpert.pe is disabled

1,164 Views
Zhuang
Contributor I

Hello Teams,

I found a very strange thing in the customer, I click the generate code, but it tells me that ProcessorExpert.pe is disabled, and my pins, peripherals, clock can not be configured, inside is gray

It also shows that the Selected processor does not support the SDK,The picture is attached.

 

0 Kudos
Reply
6 Replies

1,139 Views
Zhuang
Contributor I

微信图片_20230711161020.jpg

0 Kudos
Reply

1,131 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

do you have installed one of S32K1xx SDK (v3.0.0 or v3.0.3)? 

jiri_kral_0-1689069866116.png

 

0 Kudos
Reply

1,118 Views
Zhuang
Contributor I

Of course, my version is SDK3.0.0, and I open routines in RTD as normal.

This fault project was copied from my colleague and found that the bottom layer could not be changed.

0 Kudos
Reply

1,085 Views
jiri_kral
NXP Employee
NXP Employee

Did your colleague use the same SDK version? 

0 Kudos
Reply

1,152 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share screenshot with processor expert settings (Right click on project name -> Properties -> Processor Expert

jiri_kral_0-1689060932555.png

 

0 Kudos
Reply

1,149 Views
Zhuang
Contributor I

Hi  jiri_kral,

The attached picture is the interface where I opened Properties-Processor Expert, which shows the Selected processor does not support SDK

0 Kudos
Reply