S32DS中FreeMaster_KEAxx和KEAx_AMMCLIB两种SDK有什么区别吗?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS中FreeMaster_KEAxx和KEAx_AMMCLIB两种SDK有什么区别吗?

779 Views
cnubsq
Contributor II

如下图:

cnubsq_0-1659341953483.png

上面描述不太清楚,有人能详细点解释一下吗?

 

0 Kudos
Reply
1 Reply

774 Views
mikedoidge
NXP Employee
NXP Employee

Hello @cnubsq

The FreeMASTER and the AMMCLib are separate products. Please review the product page for each to understand fully what capabilities these products provide:

FreeMASTER Run-Time Debugging Tool | NXP Semiconductors

Automotive Math and Motor Control Library (AMMCLib) | NXP Semiconductors

The FreeMASTER Communication Driver is software code which can be included within your application project to support communication with the FreeMASTER Run-Time Debugging Tool host PC application.

I hope this answers your question.

Best Regards,

Mike