S32 design studio open fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 design studio open fail

3,314 次查看
chih-hsihsu
Contributor I

Hello, NXP Team

When I click the S32 design studio, it will show "An error has occurred.See the log file" and then the configuration folder will be created log document which is record some error information in there.

So, How could I solve this problem? 

Thanks and Regards,

CHIH-HSI

标记 (4)
0 项奖励
回复
5 回复数

3,084 次查看
chih-hsihsu
Contributor I

HI Jiri,

I follow your recommendation to delete the file but it's still doesn't work.
when click the s32ds,the message show the same things that I mentioned before.

Regards,

Chih-Hsi

0 项奖励
回复

3,084 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Chih-Hsi,

I checked again you log file - and the keylock issue is probably related to osgi container only. Please try to delete .FileTableLock file from this directory:

[Your S32DS install path]\S32_Power_v1.1\eclipse\configuration\org.eclipse.osgi\.manager\

Jiri

0 项奖励
回复

3,084 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Chih-Hsi,

Your issue is probably related to known eclipse Bug 472108. You can try to delete .FileTableLock file located on

[Your S32DS install path]\S32_Power_v1.1\eclipse\configuration\org.eclipse.core.runtime\.manager\ 

You can delete all files in this directory. Also make sure that you have rights for writing into this directory. 

Jiri 

0 项奖励
回复

3,084 次查看
chih-hsihsu
Contributor I

Hello, NXP team:

The S32DS is 1.1 version power and operating system is windows seven

Ok, please follow attachment.

0 项奖励
回复

3,084 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

Could you please clarify following points?

  • Which S32DS you use? ARM or Power? Which version?
  • Which operating system you use?
  • Could you please share the log file?

Regards,

Martin

0 项奖励
回复