S32 design studio freezes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio freezes

ソリューションへジャンプ
1,661件の閲覧回数
esmax
Contributor IV

Hello. S32 Design Studio freezes during startup and does not respond. 

there is only this window 

esmax_0-1697535456936.png

esmax_1-1697535505156.png

 

reinstallation doesn't help.

How this can be fixed?

0 件の賞賛
返信
1 解決策
1,636件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @esmax 

A possible cause for your problem could be the PC. Maybe some processes are going on in the background, causing the consumption of many resources.

You can try to reinstall the S32DS, or you also can increase the amount of memory S32DS can use as follows:

  • Locate the s32ds.ini file in C:\nxp\S32DS.3.5\eclipse and open it in a text editor.
  • Use the following options in the file to allocate more memory:
    -Xms512m
    -Xmx4096m

 

B.R.

VaneB

元の投稿で解決策を見る

2 返答(返信)
1,637件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @esmax 

A possible cause for your problem could be the PC. Maybe some processes are going on in the background, causing the consumption of many resources.

You can try to reinstall the S32DS, or you also can increase the amount of memory S32DS can use as follows:

  • Locate the s32ds.ini file in C:\nxp\S32DS.3.5\eclipse and open it in a text editor.
  • Use the following options in the file to allocate more memory:
    -Xms512m
    -Xmx4096m

 

B.R.

VaneB

1,623件の閲覧回数
esmax
Contributor IV

Thank you! Looks like it works!

0 件の賞賛
返信