S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

ソリューションへジャンプ
2,343件の閲覧回数
StarMao159376
Contributor II

Hi,Sir, S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specific optimization has been done, and can optimization be enabled?

Found in the actual project: 1 For the same 200m main frequency, mpc5744 takes more than twice as long as tc275!!!

2. However, when the optimization above O1 is enabled, the operation efficiency is significantly improved

0 件の賞賛
返信
1 解決策
2,324件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,325件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

0 件の賞賛
返信
2,304件の閲覧回数
StarMao159376
Contributor II

Thanks.

0 件の賞賛
返信