S32 Studio Compile Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Studio Compile Error

4,016 次查看
qiaodeng
Contributor II

Hi,

   I encountered the following error when compiling my project using S32:

pastedImage_1.png

What does that mean? How should I handle this?

Regards,

Qiao

标签 (1)
0 项奖励
回复
5 回复数

3,599 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

error Unsupported relocation against PIR or r4 is caused by incorrect syntax. If you use inline assembler and GPR registers, you have to use following syntax:

asm("e_li  %r0, 0");

There must be character % near the SPR register name.

Hope it helps.

Regards,

Martin

3,599 次查看
qiaodeng
Contributor II

Hi Martin,

I've found them and add % , now only the PIR error left. How should I deal with this? Thanks!

pastedImage_1.png

Regards,

Qiao

0 项奖励
回复

3,599 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I do not know, which microcontroller you use, but PIR register is special purpose register. You have to look to the core reference manual for appropriate core and find the number of the PIR register which you use instead of PIR.

Regards,

Martin

0 项奖励
回复

3,599 次查看
qiaodeng
Contributor II

Hi Martin,

     The MCU is MPC5746R, the code file is from MCAL , I just import  them into my project and don't know why they can not be complied.

Regards,

Qiao

0 项奖励
回复

3,599 次查看
stepank
Contributor I

May be you have swapped operands for this instruction ? It is common error of newbies.

0 项奖励
回复