S32_SDK_MPC574xx_EAR_0.8.2 pin_mux Bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32_SDK_MPC574xx_EAR_0.8.2 pin_mux Bug

785 Views
jeromeli
Contributor II

It is interesting that when I selected PC[5] for USB_0 and PE[7] for uSDHC, I got a conflict error. This does not happen in version 0.8.1. Is it a bug? Is there any workaround for this problem?

pastedImage_1.png

0 Kudos
2 Replies

582 Views
stanish
NXP Employee
NXP Employee

Hi Jerome,

Thanks for the report. This is a known issue which should be fixed in the next release of S32 PA SDK v0.9.0 (should be released this March). We will inform about the release on community.

The workaround is to manually write the configuration structure for that pin and use PINS_DRV_Init to apply that configuration.

BR,

Stan

0 Kudos

582 Views
jeromeli
Contributor II

Hi Stanislav,

Got it. Thanks for the reply!

Cheers,

Jerome

0 Kudos