asap
		
			asap
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I have installed the S32DS3.4, and get the S32 Flash Tool user guide from the S32DS installation folder. just found this doc (S32FTUG) only have two devices supported: S32V234 and S32S247.
could you please confirm S32 FT have supported S32G2 to program the external flash? And if so could be a way to include that info into the ug? ....
Solved! Go to Solution.
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @asap / Albert,
Once the S32G is announced for mass market, we can include references to it in the main documentation. As I understand the mass market launch for S32G is now scheduled for the beginning of May 2021.
Best Regards,
Mike
Hi,
Could anyone please share the S32 Flash tool exe file. I am unable to find it anywhere. Thank you.
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
After you install S32 Design Studio for S32 Platform, you will find the S32 Flash Tool located within the installation directory:
C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool
There are options for both GUI and command line:
"C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\GUI\s32ft.exe"
"C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\bin\S32FlashTool.exe"
Best Regards,
Mike
Thanks Mike, understood.
Hello.
I'm working with S32G and have just encountered the same problem with Flash Tool. There are only two targets: S32S247TV and S32V234.
I think I installed S32DS for S32G, version 3.5. FlashTool's help file mentions how to add other targets by referring some document that are nowhere to find.
I'd be grateful for any tips on how to add S32G target to Flash Tool.
Thanks
Michal
 asap
		
			asap
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Michal,
you may refer to the on demand training :
from 30' there is a detail S32 flash tool for S32G explaination.
albert
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello @MichalMatyl,
The S32 Flash Tool includes S32V234 and S32S247TV with the base install, for additional devices support, you are required to install the respective S32DS Development Package.
In the case of S32G, this would be 'S32G development package', latest version for S32DS 3.5 is version 3.5.2.
Best Regards,
Mike
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I was a bit confused by your details, after reading a few times, I think I understand what you are trying to do. You are using a custom board, not NXP EVB, and it has 2 flash memory devices connected via QSPI. Your board is also setup to use the Serial RCON, which means the configuration comes from the value programmed to EEPROM (as is an option with the NXP EVB). We already have a script for this to change the value, probably you already know of this:
HOWTO: Program Serial RCON using S32 Debug Probe S32G2xx
I suppose since it requires having S32 Debug Probe connected to the board via JTAG, and you noted that you need some option aside from debugger, that this is the issue you are faced with?
Unfortunately, we do not have a solution outside of this method. I will check if our developers could consider if there would be any other way to accomplish this.
What is the reason you are unable to use the Debugger/JTAG method?
 asap
		
			asap
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		thank Patrick, Mike,
my request is that if the tool is supporting S32G, we should mention it in somewhere. like the user guide in the folder "C:\NXP\S32DS.3.4\S32DS\tools\S32FlashTool\doc", we only mentioned S32S247TV and S32V234, not mentioning S32G at all. though we do have another txt file in the same folder "supported S32G devices" mentioned briefly the S32G rev1.0 rev 2.0 and 4 family members supported. can we include those info into same user guide?
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @asap / Albert,
Once the S32G is announced for mass market, we can include references to it in the main documentation. As I understand the mass market launch for S32G is now scheduled for the beginning of May 2021.
Best Regards,
Mike
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello @asap ,
The S32G support is included when the S32G2xx development package is installed. You can locate this within the Automotive SW – S32G2 Standard Software section of the NXP Flexera download site. From there, follow the link to Automotive SW - S32G2 - S32 Design Studio, then look for:
Hope that helps,
Mike
 PatrickMenter
		
			PatrickMenter
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Albert,
The tool supports all the latest, what is available publicly is limited, because not all devices have launched publicly yet. Please contact @mikedoidge and he can help you.
-Patrick