S32 Flash Tool : Failure to establish communication with target device.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Flash Tool : Failure to establish communication with target device.

1,535 次查看
Simon_Li
Contributor I

HI NXP

When I refer to the AN13750 documentation: Deployment on s32g-vnp-rdb2. 

The flash tool can't load success. Can you help me, Tks!

Refer content:

Simon_Li_0-1699430088824.png

Flash Tool failed to establish

Simon_Li_1-1699430200796.png

RDB2 SW10-1 and SW10-2 all OFF

Simon_Li_2-1699430351050.png

USB cable is OK, Because when I change sw10-2 to on, the serial output normal log.

Simon_Li_3-1699430502411.png

Thanks!

 

0 项奖励
回复
1 回复

1,487 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Simon_Li , 

 

Please can you share your project file. (you can send private message to us in the community. ) 

 

We will try the project on the hardware on our side if it works. 

 

 

By the time, please can you also check this posts if any help for your issue: 

https://community.nxp.com/t5/S32G/How-to-program-flash-the-s32g274a-board/m-p/1390281

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Im...

 

Thank you, Best regards. 

-Mehul Patel

 

0 项奖励
回复