S32 Design tool Launching issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design tool Launching issue

Jump to solution
548 Views
KarthickArumin
Contributor I

Hello Community,

As I am start to work with NXP s32 design studio IDE for my Clients32_IDE.png project, I have installed s32 IDE after installation I trying to open the IDE,but facing the issue. Kindly help me on this Please find the attachment. 

0 Kudos
Reply
1 Solution
523 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @KarthickArumin 

The issue you are encountering seems to be related to an installation problem. To help diagnose this, it would be useful to review the installation logs from both the base tool and any associated packages.

You can find the installation logs in the following directories:
- C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs\S32_Design_Studio_for_S32_Platform_3.6.0_Install_MM_DD_YYYY (date)_HH_MM_SS(time).log
- C:\Users\workspaceS32DS.3.6\.metadata\.log

If you prefer, you can also try reinstalling S32 Design Studio to resolve the issue.

 

BR, VaneB

View solution in original post

0 Kudos
Reply
1 Reply
524 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @KarthickArumin 

The issue you are encountering seems to be related to an installation problem. To help diagnose this, it would be useful to review the installation logs from both the base tool and any associated packages.

You can find the installation logs in the following directories:
- C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs\S32_Design_Studio_for_S32_Platform_3.6.0_Install_MM_DD_YYYY (date)_HH_MM_SS(time).log
- C:\Users\workspaceS32DS.3.6\.metadata\.log

If you prefer, you can also try reinstalling S32 Design Studio to resolve the issue.

 

BR, VaneB

0 Kudos
Reply