S32 Design studio - Debugger and linker folder disabled in the project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design studio - Debugger and linker folder disabled in the project

2,972件の閲覧回数
Parthasarathi_Pandiyan
Contributor I

Hi,

I installed S32 Design Studio V2.2 yesterday and tried to create a new application project. Project was created but the debugger and linker folder got disabled (please refer the screenshot attached for the reference). I added the source files and include files then added library paths. Build also able to do (no errors) and also able to flash the software to the Hardware board. When I try to keep a breakpoint before executing the program on board, it is not allowing me to keep a breakpoint. I thought due to this folder disabled, I could not keep a breakpoint before executing the program on board.

Kindly suggest me if I am doing anything wrong or anything is missed out during creation of new application project and also in adding library paths.

Thanks in advance for any support to resolve this.

0 件の賞賛
返信
2 返答(返信)

2,078件の閲覧回数
HungNguyen1001
Contributor I

I add new folder to project and my folder also be disabled like that. How can I resolve this problem.

 

0 件の賞賛
返信

2,958件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

 

the folders are "disabled" because files inside aren't part of build process. There is no relation with breakpoints. So, can you share more details about your break point issue? If you set break point to some line and start debug session, the BP disappears or what's exactly your issue? 

 

Jiri 

0 件の賞賛
返信