S32 Design Studo for ARM - Error: Program "" not found in PATH - S32K142_EVB_JumpStart_Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studo for ARM - Error: Program "" not found in PATH - S32K142_EVB_JumpStart_Firmware

6,377 次查看
Bernez
Contributor II

Hello,

I downloaded the project "S32K142_EVB_JumpStart_Firmware" from the NXP site. When I try to compile it with S32 Design Studio for ARM 2.2, I get the following error:

Bernez_0-1706779232210.png

I tried to compile the same project with S32 Design Studio for Platform, the problem is exactly the same.

Info: in both cases, I have uploaded the project by the menu "File > Open Projects from File System...".

Can you help me resolve this issue? Thank you very much.

0 项奖励
回复
14 回复数

6,263 次查看
Bernez
Contributor II

Hi Julián,

I finally managed to install version 2.0 of S32 Design Studio for ARM using my admin account. I imported the project "S32K142_EVB_JumpStart_Firmware", but the generation results in the same error as with version 2.2. Here is the screenshot:

Bernez_1-1707304308137.png

 

In case this could be useful to help me resolve this problem, the installation log file is attached.

Once again thank you for your help.

Bernard.

 

0 项奖励
回复

6,231 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

Could you help me confirm you installed SDK_S32K14x_08 and followed Q&A of S32K1x FreeMASTER JumpStart Project?

If the project still doesn't work, you can try the following community post:

Please update me on any findings.

Best regards,
Julián.

0 项奖励
回复

6,208 次查看
Bernez
Contributor II

Hi Julián,

yes I tried to follow "Q&A of S32K1x FreeMASTER JumpStart Project", but everything is not working properly. In the "4.5 Set Up Debug Configuration" chapter, the "Apply" button is not active, only the "Debug" button is accessible. When you click on it, an error message appears.

Bernez_1-1707385865097.png

 

Bernez_0-1707385791196.png

When I proceed:

Bernez_2-1707386015388.png

Click on "Yes":

Bernez_0-1707405393776.png

it seems that we can debug (Run, Suspend, Resume, Step Into, Step Over, Step Return, Terminate… are available), but we do not have access to the source files, it is not viable. I don't know where the indicated path is found ("D:\GIT\033_jumpstart_sw\S32K142_EVB_JumpStart\S32K142_EVB_JumpStart_Firmware\Debug_FLASH/../Sources/main.c"), I looked in the paths specified in the project properties, this path is not specified anywhere, and it does not appear in the source files (according to what I could find).

Yes, I updated "S32 Design Studio for Arm® v2.0 Update 2 – S32 SDK 0.8.5 EAR & MQX", here are the installation details:

Bernez_4-1707389514076.png

I reconfigured the baud rate to 115200 as indicated in chapter 4:

Bernez_1-1707405495980.png

 

and then I clicked Generate Processor Expert Code:

Bernez_8-1707391046349.png

The problem is still the same.

I had already read the community posts, but the only information that seemed interesting to me would be a command line exceeding 8192 characters and that the GNU ARM Eclipse build tool would have to be updated. The proposed version seems obsolete. I don't know how to check which version I'm currently using and I don't know exactly what to update. 

 

Best regards.

Bernard

 

 

 

 

 

 

0 项奖励
回复

6,098 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

Regarding to not having access to the source files when debugging, when you proceed with debugging with errors in the active configuration, the debug perspective does not function properly.

Just to confirm, there has been no modification to the example after importing, correct? I am asking this because I can build the example correctly with no modifications.

Julin_AragnM_0-1706827014278.png

Best regards,
Julián

0 项奖励
回复

6,067 次查看
Bernez
Contributor II

Hi Julián,

Yes, I confirm that there were no changes to the example after import.

Best regards.

Bernard.

0 项奖励
回复

6,051 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

Since there seems no changes in importing or environment, could you share the project to confirm this behaviour? As we cannot recreate the issue.

Best regards,
Julián

0 项奖励
回复

6,030 次查看
Bernez
Contributor II

Hi Julián,

Yes, I can share the project, here it is attached.

Best regards.

Bernard.

0 项奖励
回复

5,960 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

When importing your project, S32DS throws me many errors in configuration for the SDK, as such:

Julin_AragnM_0-1708107685007.png

As well as some path problems;

Julin_AragnM_1-1708107722128.png

This seems to be a problem with the project configuration for the KSDK specific path:

Julin_AragnM_2-1708107848712.png

Could you try installing S32 Design Studio for Arm v2.0 - Update 3, which includes S32K14x_EAR_0.8.6? This seems to fix the SDK path value issue:

Julin_AragnM_3-1708107902423.png

Once this update is installed, please try importing the project I have shared into the workspace, the same way you already explained in the original post: Import > Existing Project Into Workspace > Select archive file > Finish

Once imported, move the Baudrate configuration first, generate Processor Expert Code which should prompt a "Track Changes" window:

Julin_AragnM_4-1708108182778.png

After accepting and waiting for the code to be generated, the project should be able to be built:

Julin_AragnM_5-1708108220632.png

If this is still not the case, I would suggest reinstalling S32DS, and only adding update 2 and 3, and testing these steps again, as your workspace or installation may have been broken.

I have also added the build log, and some project properties for the C Build, as you error seems to be related to the makefile, so you can compare:

Julin_AragnM_10-1708108446794.png

Julin_AragnM_9-1708108435715.png

Best regards,
Julián.

0 项奖励
回复

5,869 次查看
Bernez
Contributor II

Hi Julián,

I have installed S32 Design Studio for Arm v2.0 - Update 3, which includes S32K14x_EAR_0.8.6. I then updated the project configuration for the KSDK specific path as you requested. The operation went well.

I then wanted to import the project that you just shared with me, but this is not possible because projects cannot be imported when they already exist in the workspace. So I deleted the old project from the workspace so I could import the new one.

Bernez_0-1708358501807.png

but the following error appeared:

Bernez_1-1708358522280.png

No action is then possible, an error systematically occurs.

So I decided to uninstall then reinstall S32DS and add update 3:

Bernez_2-1708358554713.png

Bernez_3-1708358576884.png

Bernez_6-1708358733464.png

Bernez_7-1708358758334.png

Bernez_8-1708358778828.png

After that, I built the project, there are no more errors but there are still 7 warnings. I will now try to resolve them.

Bernez_10-1708359084801.png

Bernez_9-1708359014180.png

Bernard.

0 项奖励
回复

5,855 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

I'm glad there are no more errors when building. You can still flash and debug the code if there are just warnings in the workspace.

I hope you found this helpful.

Best regards,
Julián

0 项奖励
回复

6,290 次查看
Bernez
Contributor II

Hi Julián,

I think the installation went wrong because I didn't run as administrator. I'll start again, but I won't have time to do it until tomorrow morning. Wait to answer me, I'll give you news tomorrow. Excuse me for the disruption.

Best regards.

Bernard.

6,286 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

No problem, please update me on any findings.

If this was a permission error, inside the nxp folder, under "C:\nxp\S32DS_ARM_v2.0\_S32 Design Studio for ARM v2.0_installation\Logs" you can find the .log file containing the following line:

Julin_AragnM_1-1707242831018.png

 

I will be waiting for your answer.

Best regards,
Julián.

0 项奖励
回复

6,309 次查看
Bernez
Contributor II

Hi Julián,

Thank you for your reply. I downloaded version 2.0 of S32 DS ("S32DS_ARM_Win32_v2.0_b170810.exe"). Unfortunately the installation does not go well, here is the message I get:

Bernez_0-1707217628712.png

What is the problem, do I need to uninstall version 2.2 first?

Best regards.

Bernard.

 

0 项奖励
回复

6,348 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Bernez,

The S32K142 EVB JumpStart firmware was made for S32 Design Studio for ARM v2.0. Please try to compile the project on this SW version:

Julin_AragnM_0-1706827014278.png

It is also required to install SDK_S32K14x_08, and to reconfigure the baud rate to 115200 as explained in the Q&A of S32K1x FreeMASTER JumpStart Project from the community post.

Hope you find this helpful.

Best regards,
Julián.

 

0 项奖励
回复