Hi,
On task manager:
Memory Used: 20% for Everything
Network Activity: approx 0%
CPU Load: < 6% for everything
WmiPrvSv.exe is the task most using the CPU at around 2%
DS is second most active at 0.5%
After exiting the PC is unusable until rebooted (IE, Firefox, Windows Explorer do not open any windows when trying to start them).
Running make -j4 clean from the command line is fine (< 1sec), provided that DS is not started since powering on the PC.
Running DS, exiting, and then running make from the command line, is very slow (> 15mins)
Uninstalling DS, rebooting and reinstalling DS has no effect.
Removing Visual Studio has no effect.
Any ideas appreciated.
Dermot