S32 Design Studio for Power Architecture v2.1 Update 14 could not be installed Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power Architecture v2.1 Update 14 could not be installed Error

732 Views
GianpieroTrane
Contributor I

Hello,

I'm trying to install the S32 Design Studio for Power Architecture v2.1 Update 14. I followed the instructions in https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architectu... from @mikedoidge.

I tried both Online and Offline Update in S32DS Extensions and Updates. None of them works.

In both cases when I select Update with S32 SDK 1.0.0 RTM for S32R294 for Power Architecture version 2.1.14 and click Install/Update, I get a new window showing "Cannot perform operation. Computing alternative solutions"

The error log shows "From: S32R294 development package 1.0.0.202011241025 (com.nxp.s32ds.s32r294.dev.feature.feature.group 1.0.0.202011241025). Software being installed: S32R294 development package 1.0.0.202011241025 (com.nxp.s32ds.s32r294.dev.feature.feature.group 1.0.0.202011241025)."

I tried Update 13 and it was installed without problems, but update 14 just doesn't work.

Thanks,

Gianpiero Trane

0 Kudos
1 Reply

711 Views
GianpieroTrane
Contributor I

Solved my issue by using the option to Install New Software instead of the S32DS Extensions and Updates interface. It's a bug to solve though. 

0 Kudos