S32 Design Studio for Power Architecture Version 2.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio for Power Architecture Version 2.1

1,563 次查看
PENGHAN
Contributor II

Dear

      The processor I use is MPC5777C, the debuger I use is Multilink_Universal_FX, and the IDE I use is S32 Design Studio for Power Architecture Version 2.1.I created the project to be able to debug in RAM and flash.

      But I can't download the generated .elf file to flash using the flash from file tool.Attached is the .elf file generated by the project.The compilation information of the console is as follows:

       “Connection from "127.0.0.1" via 127.0.0.1. Connection from port "49779" to 7224
Copyright 2018 P&E Microcomputer Systems,Inc.
Command Line :D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port�
P&E Interface detected - Flash Version 10.81
Flash Data in range 0x00800000-0x00800007.
Flash Data in range 0x00800400-0x008006ED.
Flash Data in range 0x00810000-0x008100F3.
Flash Data in range 0x00811000-0x00811763.
Flash Data in range 0x00811770-0x0081B453.

CMD>RE

Initializing.

Device IDCODE is $00000377
Device ID revision is $00000001
Initializing Ram Block 0x00300000-0x00307FFF.
MPC5777C Device detected.
Target has been RESET and is active.
CMD>CM D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp

Initializing.

Device IDCODE is $00000377
Device ID revision is $00000001
Initializing Ram Block 0x00300000-0x00307FFF.
MPC5777C Device detected.

DOUBLE BUFFERING enabled.
Initialized.

;version 1.04, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [5777C_8meg_highspeed]

;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed

;begin_cs device=$30800000, length=$00800000, ram=$00300000

Loading programming algorithm ...
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00800000-00800007 ...
Ok.
block 00800400-008006ED ...
Ok.
block 00810000-008100F3 ...
Ok.
block 00811000-00811763 ...
Ok.
block 00811770-0081B453 ...
Ok.
Checksum Verification Successful. (Cumulative CRC-16=$9609)
Application verified in memory. No need to reprogram.

CMD>RE

Initializing.

Device IDCODE is $00000377
Device ID revision is $00000001
Initializing Ram Block 0x00300000-0x00307FFF.
MPC5777C Device detected.
Target has been RESET and is active.

Device IDCODE is $00000377
Device ID revision is $00000001

Starting reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\s32e200_mpc5777c.mac) ...
REM This script is compatible with MPC5777C devices.
REM Clean GPRs to remove residual data after using algorithm
REM Setup MMU for for Periph B Modules
REM Base address = $FFE0_0000
REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access
Once Status Register Result = $0209
REM Set up MMU to put internal Flash at 0...
REM Virtual address 0x0 -> Physical address = $0000_0000
REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access
Once Status Register Result = $0209
REM Set up MMU for External Memory
REM Base address = $2000_0000
REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access
Once Status Register Result = $0209
REM Set up MMU for Internal SRAM
REM Base address = $4000_0000
REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access
Once Status Register Result = $0209
REM Set up MMU for Periph A Modules
REM Base address = $C3E0_0000
REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access
Once Status Register Result = $0209
REM Initialize all of the Main SRAM - 512KB
Initializing RAM from $40000000 to $4007FFFF.
Initializing Ram Block 0x40000000-0x4007FFFF.

Reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\s32e200_mpc5777c.mac) completed.

MPC5777C Device detected.
No breakpoints currently set.
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "49779" from 7224
Target Disconnected.

 

1.PNG2.PNG

       I really need your help, thank you very much for your help.

        respectly

0 项奖励
回复
1 回复

1,540 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Penghan,

It's not clear what the issue is here. The log you provided shows a successful flashing event from using the Flash from File utility. The images you shared are displaying the result of successfully starting a debug session. Each of these is from separate, unrelated, actions. Are you trying to flash or debug? Both appear to be working well.

Perhaps there is some misunderstanding?

Best Regards,

Mike

0 项奖励
回复