S32 Design Studio for ARM license expiring in 13 days

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for ARM license expiring in 13 days

ソリューションへジャンプ
18,385件の閲覧回数
609510318
Contributor I

S32 Design Studio for ARM license expiring in 13 days,how can i solve it?Thanks!

 

S32 Design Studio for ARM

ActivationId: F625-BD17-9FB6-009D
Evaluation Days: 13
Feature Version: 2.2
Feature Status: Evaluation (13 days)

0 件の賞賛
返信
1 解決策
18,264件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

I have returned your license, when you re-activate, the new expiration date will be loaded.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
68 返答(返信)
3,977件の閲覧回数
Romeo
Contributor I

Hi Mike,

I made the KEA8 firmware using S32 Design Studio for ARM v2.2 3 year free license.
The current project is over.
We are currently selling products with firmware (*.srec) created by the project.
When the license expires, will I be unable to sell products made with the current firmware?

Best Regards,

romeo

0 件の賞賛
返信
3,958件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Romeo,

I believe you are confusing the Software License Agreement with the Software Tools License.

The Software License Agreement covers how the software you develop using the NXP provided SDKs may be used and distributed. The terms and conditions you agreed to when you installed the SDK specify the limitations. I'm not aware there is a defined time limit, but you should review this agreement to ensure you understand the limitations and that you are in compliance.

The Software Tool License for S32 Design Studio is what enables you to activate and make use of the IDE for development purposes. You cannot use the IDE without an active license. This license is generally provided with expiration of 3 years, however, we can extend the tool license for you at any time.

I hope this answers your question.

Best Regards,

Mike

 

0 件の賞賛
返信
5,085件の閲覧回数
Att1l10
Contributor I

Sorry, I have the same issue for

S32 Design Studio for ARM v2018 R1

Activation code: E281-F80C-438F-6887

Please, could you renew also it.

Thanks

0 件の賞賛
返信
5,080件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

This one has been renewed through 2025. Please re-activate your installation.

Best Regards,

Mike

0 件の賞賛
返信
5,374件の閲覧回数
markus1
Contributor II

Hi NXP-Team,

my license has expired too. Can you please help me with that?

Best regards,

Markus

0 件の賞賛
返信
5,348件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Markus,

I have extended your entitlement through 2025. Please re-activate your installation.

Best Regards,

Mike

0 件の賞賛
返信
5,751件の閲覧回数
jonaspause
Contributor I

Hi, I have the same issue:

Fulfillment ID: 153510107
Expiration Date: Aug 1, 2022
Product: S32 Design Studio for ARM v2018 R1
Machine: 70990A1E3F1FE8C48BAD3BAF14F6163E9DA45CDC
Activation Code: CE54-8A45-DFCB-2A14

0 件の賞賛
返信
5,748件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Jonas,

I have extended your entitlement. Since your license has already expired, you probably won't be able to refresh. You will need to re-activate using the existing activation code. It should prompt you when you launch S32 Design Studio.

Best Regards,

Mike

6,316件の閲覧回数
renzoquaglieri
Contributor I

Hi my license is expired too. Can you extend it? thank you!

S32 Design Studio for PA E200 v2.0
4A7F-2866-9BBB-431E

0 件の賞賛
返信
6,288件の閲覧回数
chrislin_wpi
Contributor II

It needs NXP Employee to extend.

0 件の賞賛
返信
6,307件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

Your license was extended through 2025.

Please refresh or reactivate your license.

Best Regards,

Mike

0 件の賞賛
返信
6,598件の閲覧回数
ArturG
Contributor I

Same problem here, license expired, cant renew the license.

ActivationID: D70F-D40C-4AD2-DF97

Version 2018.R1

Can somebody help me with this?

 

@mikedoidge 

0 件の賞賛
返信
6,594件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Artur,

I have extended your entitlement through 2025. Please refresh the license from within the Help->NXP Licenses menu. Or you might have to return and re-activate using same activation code as before.

Please let me know of any further issue.

Best Regards,

Mike

0 件の賞賛
返信
6,169件の閲覧回数
debangshudey
Contributor I

Hi, 
I would like my license extended as well.

License Applicable to Product(s):

  Version  Description
  2018  S32 Design Studio for ARM v2018 R1

 

1
194470497
Jun 4, 2022
S32 Design Studio for ARM v2018 R1

Activation Code:

CCF8-7C0D-1FEF-C281
0 件の賞賛
返信
6,159件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I extended your license till end of 2025. Please enter your activation code in S32DS again. 

 

Jiri 

0 件の賞賛
返信
6,903件の閲覧回数
vlele
Contributor II

Hi Mike,

Kindly renew 

Fulfillment ID:

192400897

Expiration Date:

Mar 15, 2022

Product:

S32 Design Studio for ARM v2018 R1

Machine:

6DB8562794A476A701EEF087DCDA7006DDF50E2C

Activation Code:

89AE-671C-7A13-D4D3

0 件の賞賛
返信
6,885件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

Your entitlement has been extended through 2025. Please either 'refresh' the license from the NXP Licenses menu (Help -> NXP Licenses) or re-activate using the code you shared.

Best Regards,

Mike

0 件の賞賛
返信
7,055件の閲覧回数
Rameshv
Contributor I

Hi Mike,

My S32 Design Studio for Power architecture license expired (B86D-B7D4-0C1D-3021), can you please extend it?.

0 件の賞賛
返信
7,011件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Ramesh,

I have extended your entitlement through 2025. Please refresh the license or reactivate your install.

Best Regards,

Mike

0 件の賞賛
返信
8,317件の閲覧回数
Bryan9
Contributor I

Hello

I have the same problem too.

Can you reactivate my license for S32 Design Studio for ARM V1.3, please?

Activation ID: 816A-E5D9-CA6E-E65E

0 件の賞賛
返信