S32 Design Studio and SDK 3.0 for S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio and SDK 3.0 for S32K144

6,620件の閲覧回数
alwin_lutz
Contributor II

I installed the new S32K IDE:

S32 Design Studio

Version: 3.2
Build id: 190924

I want to develop code for the S32K144 micro.

I downloaded and installed the SDK: S32SDK_S32K1xx_RTM_3.0.0.exe

How do I make this SDK available (usable) within the S32 Design Studio?

I would like to use Processor Expert and FreeRtos 10.x that is contained in the SDK.

Any help greatly appreciated...

Al

タグ(2)
0 件の賞賛
返信
6 返答(返信)

6,032件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

for S32K144 you need this version of S32DS: 

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! 

Here are details about S32DS Versions:

https://community.nxp.com/docs/DOC-335338 

Jiri

0 件の賞賛
返信

6,032件の閲覧回数
alwin_lutz
Contributor II

Hi,

thank you very much for the quick response.  By default this IDE has "Fully integrated S32 SDK for S32K14x EAR release v.0.8.6.".  How can I get the S32SDK_S32K1xx_RTM_3.0.0 instead??

0 件の賞賛
返信

6,032件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

just update it -> https://community.nxp.com/docs/DOC-344776 

Jiri

0 件の賞賛
返信

6,032件の閲覧回数
alwin_lutz
Contributor II

I am confused, I went through all the update, but it switched me back to the old FreeRTOS version "V8.2.1"

and the repository "SDK_S32K14x_09"

If I want to change the repository back to "SDK_S32K1xx_15/FreeRTOS, version SDK_S32K1xx_15" it shows me

"not supported for selected processor".  How can I get the latest??

0 件の賞賛
返信

6,032件の閲覧回数
alwin_lutz
Contributor II

I switched the repositories back to "xx_15" and now when I try to build I get a pop up message saying"

"This Processor Expert project requires KSDK 1.1 bu the Kinetis SDK path option refers to SDK_S32K14x_09? Select "Yes"

to convert or "No" to open project prefernces to change Kinetis SDK path. Select "Cancel" for no action."

What shall I do??

0 件の賞賛
返信

6,032件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share more details what you are trying to do? It looks that you are going to import some older SDK based project, Am I right?

In SDK RTM v3.0.0 is already FreeRTOS v10.0.1 example. 

Jiri

0 件の賞賛
返信