S32 Design Studio V3.4 unable to update the or add Extension

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio V3.4 unable to update the or add Extension

1,712 Views
Prem_Venkata_Subbarao
Contributor II

Hi,

I am not able to update and add Extensions required for my Project.

The link which is referenced in the tool is not reachable:  http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.4

Please let me know how to resolve this issue.

Regards,

Prem Venkata Subbarao Annam

0 Kudos
Reply
1 Reply

1,687 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

This is likely a temporary issue with the website. There are times when the website is not working to perform some updates. I would suggest trying at different times. If this will not work, then the same update packages are available for download and offline installation.

If you are unable to get the online update to work, then let us know the packages you wish to install and we can help you to locate the offline installation packages.

Best Regards,

Mike

0 Kudos
Reply