S32 Design Studio V1.2 starts failed after Offline activation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio V1.2 starts failed after Offline activation

1,223 Views
1213513998
Contributor I

S32 Design Studio V1.2 starts failed after Offline activation installation, although there is information says the installation is successful. After the installation, I double click the icon to start the S32DS V1.2 IDE on my 64bit computer, which runs on a windows 7 OS, then it appears the information"An error has occurred.See the log file D:\software\s32_power_win32_v1.2\eclipse\configuration\1587541348989.log.", when I install it on a x86 computer, it starts normally after my double click the icon.

here are the contents of log files: 

 1.  request.xml 

<?xml version="1.0" encoding="UTF-8" ?><Request xmlns="http://www.macrovision.com/fnp/2004/11/activation"><RequestHeader><VersionNumber>3</VersionNumber><RequestType>ACTIVATION</RequestType></RequestHeader><RequestData><EntitlementData>
<EntitlementId>F5C1-454F-0B3F-D638</EntitlementId>
<ActivationReason>0</ActivationReason>
<ProductId>Not Applicable</ProductId><PublisherId>10295808</PublisherId>
</EntitlementData><OriginData><ClientVersion>11.13.0</ClientVersion><ConfigData><IsServer>0</IsServer><TrustedHostInformation><TrustedId>3</TrustedId><Revision>1</Revision><RevisionType>SRV</RevisionType><MachineIdentifier>C10B71177DE41388FFF8D8F63272A257460555DE</MachineIdentifier><Status>OK</Status></TrustedHostInformation></ConfigData>
<Platform>
<PlatformTypeName>i86_n3</PlatformTypeName>
<OperatingSystem><Info>none</Info></OperatingSystem>
</Platform>
<UniqueMachineNumbers>
<UniqueMachineNumber><Type>1</Type><Value>DD27C1ECE3C53BD3AF0066FECCEDDE48B08EBBB8</Value></UniqueMachineNumber>
<UniqueMachineNumber><Type>2</Type><Value>8DA5DC9D43A2734F9CFB439C9AAF6E918F126C23</Value></UniqueMachineNumber>
</UniqueMachineNumbers>
<SequenceNumber>1</SequenceNumber></OriginData><PublisherDictionary>
<Entries>
<Entry>
<Key>flexFulfillmentVersion</Key>
<Value>1</Value>
</Entry>
</Entries>
</PublisherDictionary></RequestData><Hash>36D5F97454FB2C75A57499FC6A34B353E6F1553C</Hash><HashVersion>1</HashVersion></Request>

2.  activation.xml 

<?xml version="1.0" encoding="UTF-8" ?><Response xmlns="http://www.macrovision.com/fnp/2004/11/activation"><ResponseHeader><VersionNumber>2</VersionNumber><ResponseType>ACTIVATION</ResponseType><RequestSequenceNumber>1</RequestSequenceNumber><RequestHash>36D5F97454FB2C75A57499FC6A34B353E6F1553C</RequestHash></ResponseHeader><ResponseData><EntitlementData><EntitlementId>F5C1-454F-0B3F-D638</EntitlementId><ProductId>Not Applicable</ProductId></EntitlementData><TrustedHostInformation><TrustedId>3</TrustedId><Revision>1</Revision><RevisionType>SRV</RevisionType><MachineIdentifier>C10B71177DE41388FFF8D8F63272A257460555DE</MachineIdentifier><Status>OK</Status></TrustedHostInformation><FulfillmentRecord><FulfillmentRecordHeader><VersionNumber>1</VersionNumber></FulfillmentRecordHeader><FulfillmentRecordData><FulfillmentId>172921657</FulfillmentId><FulfillmentDictionary><Entries><Entry><Key>serverHostId</Key><Value>INTERNET=0.0.0.0</Value></Entry><Entry><Key>fulfillmentIdChain</Key><Value>172921657</Value></Entry><Entry><Key>servOrLocal</Key><Value>2</Value></Entry><Entry><Key>availAct</Key><Value>1</Value></Entry><Entry><Key>fulfillmentType</Key><Value>6</Value></Entry><Entry><Key>actServerChain</Key><Value>https://nxp.flexnetoperations.com/control/frse/ActivationService</Value></Entry><Entry><Key>features</Key><Value>INCREMENT Activated freescale 1.2 16-jun-2023 1 \
VENDOR_STRING=S32-DS-E200_v1.2|F5C1-454F-0B3F-D638|NO_TRIAL \
DUP_GROUP=UHDV ISSUER="Freescale Semiconductor" \
ISSUED=22-apr-2020 ck=129 SN="FSL - 30328777" TS_OK SIGN="0296 \
8025 ACEC 5534 B687 E3DE D973 B0A1 8D15 1B55 1777 7F25 3555 \
602C 396C 11F6 D87B DC00 5A6C 1218 7276 19E0 D2B2 C66F 5780 \
6286 CC44 D71D 387D 5216"
</Value></Entry><Entry><Key>expiry</Key><Value>16-Jun-2023</Value></Entry><Entry><Key>productId</Key><Value>S32-DS-E200_v1.2</Value></Entry><Entry><Key>entitlementId</Key><Value>F5C1-454F-0B3F-D638</Value></Entry></Entries></FulfillmentDictionary></FulfillmentRecordData></FulfillmentRecord></ResponseData><Signature>0FA674232B263BB9B97E4DD99150D291CF78673E5245FA5012A37E72F55E13CA62F1D7ADF8AAA524505FD31C6C11FEC770C64C9333F88A29EE090292</Signature><SignatureVersion>1</SignatureVersion></Response>

3.  1587541348989.log

!SESSION 2020-04-22 15:42:28.833 -----------------------------------------------
eclipse.buildId=4.4.2.M20150204-1700
java.version=1.8.0_51
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=zh_CN
Framework arguments: -product com.freescale.s32ds.e200.ide
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.freescale.s32ds.e200.ide

.......

.......

!ENTRY org.eclipse.osgi 4 0 2020-04-22 15:42:38.661
!MESSAGE Application error
!STACK 1
java.lang.RuntimeException: Application "org.eclipse.ui.ide.workbench" could not be found in the registry. The applications available are: org.eclipse.ant.core.antRunner, org.eclipse.cdt.codan.core.application, org.eclipse.cdt.core.GeneratePDOM, org.eclipse.equinox.app.error, org.eclipse.equinox.p2.director, org.eclipse.equinox.p2.garbagecollector.application, org.eclipse.equinox.p2.publisher.InstallPublisher, org.eclipse.equinox.p2.publisher.EclipseGenerator, org.eclipse.equinox.p2.publisher.ProductPublisher, org.eclipse.equinox.p2.publisher.FeaturesAndBundlesPublisher, org.eclipse.equinox.p2.reconciler.application, org.eclipse.equinox.p2.repository.repo2runnable, org.eclipse.equinox.p2.repository.metadataverifier, org.eclipse.equinox.p2.artifact.repository.mirrorApplication, org.eclipse.equinox.p2.metadata.repository.mirrorApplication, org.eclipse.equinox.p2.updatesite.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.CategoryPublisher, org.eclipse.help.base.infocenterApplication, org.eclipse.help.base.helpApplication, org.eclipse.help.base.indexTool, org.eclipse.jdt.core.JavaCodeFormatter, org.eclipse.jdt.core.JavaIndexer.
at org.eclipse.equinox.internal.app.EclipseAppContainer.startDefaultApp(EclipseAppContainer.java:248)
at org.eclipse.equinox.internal.app.MainApplicationLauncher.run(MainApplicationLauncher.java:29)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:380)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:235)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:648)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:603)
at org.eclipse.equinox.launcher.Main.run(Main.java:1465)

How to solve this problem under an Offline activation installation method? 

Thank you.

                                                                                                                                       yours Jakie. 

0 Kudos
Reply
2 Replies

1,065 Views
mikedoidge
NXP Employee
NXP Employee

Hello 1213513998@qq.com‌,

Could you please try the solution here: Troubleshooting: S32 Design Studio exits unexpectedly or Installer rolls back immediately following ...

It may not be exact scenario described there, but it could help to try it.

I also have a question for you. Is it possible you could migrate to the new version of the S32 Design Studio for Power Architecture v2.1? It has many bug fixes and improvements. This issue may be resolve for you in this new version.

Hope it helps,

Mike

0 Kudos
Reply

1,065 Views
1213513998
Contributor I

Thanks for your advice, Mike, I'll try it. 

Jakie 

0 Kudos
Reply