Hello,
I have a question I want to ask. I have a project in S32 Design Studio which is based on lwip_s32k148 example. I want to upload this project on GIT. But problems is when I upload the source code. The lwip stack is not copied but linked to s32 design studio libraries. For example the folder middleware/lwip/src/api is empty. I cant see anything there.
Previously I have been using Kinetis Design Studio and MCUExproso in which the code whole content of the example project was copied into work spaces. This is a real problem especially if you are uploading the code on GIT. What can be done about this