S32 DS v2.2 processor expert error messages

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 DS v2.2 processor expert error messages

850 次查看
cuongtran
Contributor II

when I start opening a project in S32 DS V2.2, the following messages showed up.  Does any one know why??

and how can  I get rid of these error messages?.  Thanks.

标记 (2)
2 回复数

770 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your project? It is an example or some old project which you like to migrate into new S32DS? 

Jiri

0 项奖励
回复

770 次查看
cuongtran
Contributor II

It is new project with adding lpspi component from processor expert. I also notice that when I open the project with lpspi component, these error message will pop up as well.

This is not happen for this v2.2 DS, it is also happen on R2018.R1 DS as well. However, there was no error during compilation of the code and code working as I expected.

I am not too concern about this, but just want to know why.

Thanks.

Cuong.