Dear NXP experts:
Could you do me a favor to support me on this S32 Design Studio issue?
the MCU is MPC5746R, S32 Design Studio V2.1, the CORE0 project can be built successfully.
But forCORE1 project , there're following Errors, and no hint to fix:
1) several files can't be built
2) files like flashrchw.c, main_Z4_1.c can't be added into build path-debug, there is a '/'

thanks and BR
YiChuan