S32 DS KEA-128 Open Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS KEA-128 Open Project

2,478 Views
ugurozkan52
Contributor II

Hi everyone,

I have a TRK-KEA128 i am using S32DS for TRK programing but S32 DS is not found device how can i solve ? Regards

148922_148922.pngEkran Görüntüsü (3).png

8 Replies

1,462 Views
ugurozkan52
Contributor II

Hi Yunus,

I am sorry for I couldn't answer your question.

I couldn't solve problem. I desided using Code Warrior and Kinetis Design Studio.

Regards,

Uğur

0 Kudos

1,462 Views
vigneshbalaji
Senior Contributor I

Hi,

    what is the advantage of using S32 over KDS or codeWarrior?

0 Kudos

1,462 Views
yunus_ozdemir
Contributor I

Hi,

Did you solve the problem Uğur? Unfortunately, I got same problem and still trying to solve.

Yunus.

0 Kudos

1,462 Views
ugurozkan52
Contributor II

Hi,

I using Windows 10 and have java version 8 update 92

I will try me too

Thanks for your concern,

Ugur

issue

0 Kudos

1,462 Views
ugurozkan52
Contributor II

Hi,

Alice_Yang Thank you for your suggestion. I will try Kinetis Desing Studio IDE.

Martin Kovar ​I have S32 Design Studio for ARM Version: 1.2 but when I created new project I didn't see your table. I activeted from site of nxp. Did you create kinetis-sdk or any patchs also did you update anything.

Adsız.png

Thanks for your concern.


0 Kudos

1,462 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I uninstalled all versions of S32DS for ARM and installed just version 1.2 and I cannot still reproduce your problem. I have only installation of S32 without any updates, patches or SDK.

Could you please tell me, which OS you use? Also please write me, what is your Java version. I will try to find you the issue.

Regards,

Martin

1,462 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please specify, which version of S32DS you use? I have installed S32DS version 1.2 and when I create new project, I see this table:

pastedImage_0.png

Have you activate your installation?

Regards,

Martin

1,462 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

You can use the KDS IDE, it is free and it support this chip,

and it is easy to used.

you can download it at here :

Kinetis Design Studio Integrated Development Enviro|NXP

Hope it helps

Alice

0 Kudos