S-record (S2 v S3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S-record (S2 v S3)

Jump to solution
2,656 Views
jackboatman
Contributor II

Using S32DS for MPC5777C. Default /example project. In Properties>ToolSettings>CrossSettings I have Create flash image checked. Under create flash image>General I have Motorola S-rec selected. When I build I get the s-rec. But it is always S2. How can I get S3?

Labels (1)
0 Kudos
1 Solution
6 Replies
2,437 Views
jackboatman
Contributor II

Fantastic, that does it. Thank you very much.

0 Kudos
2,437 Views
jackboatman
Contributor II

I would be happy to try that. But I do not know where I would put that line / command; hardware guy writing test code.

0 Kudos
2,438 Views
alexanderfedoto
NXP Employee
NXP Employee

pastedImage_1.png

2,437 Views
jackboatman
Contributor II

Fantastic. Thank you.

Jack

0 Kudos
2,436 Views
alexanderfedoto
NXP Employee
NXP Employee

Have you tried "--srec-forceS3" ?

0 Kudos
2,436 Views
jackboatman
Contributor II

Thanks, I’d be happy to try, but I don’t know where to put that line/command; hardware guy writing test code.

Jack

0 Kudos