S-record (S2 v S3)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S-record (S2 v S3)

跳至解决方案
2,640 次查看
jackboatman
Contributor II

Using S32DS for MPC5777C. Default /example project. In Properties>ToolSettings>CrossSettings I have Create flash image checked. Under create flash image>General I have Motorola S-rec selected. When I build I get the s-rec. But it is always S2. How can I get S3?

标签 (1)
标记 (3)
0 项奖励
1 解答
2,421 次查看
alexanderfedoto
NXP Employee
NXP Employee
6 回复数
2,421 次查看
jackboatman
Contributor II

Fantastic, that does it. Thank you very much.

0 项奖励
2,421 次查看
jackboatman
Contributor II

I would be happy to try that. But I do not know where I would put that line / command; hardware guy writing test code.

0 项奖励
2,422 次查看
alexanderfedoto
NXP Employee
NXP Employee

pastedImage_1.png

2,421 次查看
jackboatman
Contributor II

Fantastic. Thank you.

Jack

0 项奖励
2,420 次查看
alexanderfedoto
NXP Employee
NXP Employee

Have you tried "--srec-forceS3" ?

0 项奖励
2,420 次查看
jackboatman
Contributor II

Thanks, I’d be happy to try, but I don’t know where to put that line/command; hardware guy writing test code.

Jack

0 项奖励