S-record (S2 v S3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,096件の閲覧回数
jackboatman
Contributor II

Using S32DS for MPC5777C. Default /example project. In Properties>ToolSettings>CrossSettings I have Create flash image checked. Under create flash image>General I have Motorola S-rec selected. When I build I get the s-rec. But it is always S2. How can I get S3?

ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
2,877件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee
6 返答(返信)
2,877件の閲覧回数
jackboatman
Contributor II

Fantastic, that does it. Thank you very much.

0 件の賞賛
2,877件の閲覧回数
jackboatman
Contributor II

I would be happy to try that. But I do not know where I would put that line / command; hardware guy writing test code.

0 件の賞賛
2,878件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee

pastedImage_1.png

2,877件の閲覧回数
jackboatman
Contributor II

Fantastic. Thank you.

Jack

0 件の賞賛
2,876件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee

Have you tried "--srec-forceS3" ?

0 件の賞賛
2,876件の閲覧回数
jackboatman
Contributor II

Thanks, I’d be happy to try, but I don’t know where to put that line/command; hardware guy writing test code.

Jack

0 件の賞賛