Program "arm-none-eabi-g++" not found in PATH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program "arm-none-eabi-g++" not found in PATH

ソリューションへジャンプ
790件の閲覧回数
batch202563
Contributor I

Hello there,

When starting S32DS (V3.6.2), the following error occurs.

Description Resource Path Location Type
Program "arm-none-eabi-g++" not found in PATH T1_powersupply_test Project Properties, C++ Preprocessor Include.../Providers, [CDT S32DS Built-in Compiler Settings] options C/C++ Scanner Discovery Problem
Program "arm-none-eabi-gcc" not found in PATH T1_powersupply_test Project Properties, C++ Preprocessor Include.../Providers, [CDT S32DS Built-in Compiler Settings] options C/C++ Scanner Discovery Problem

However, the build itself completes successfully.

0 件の賞賛
返信
1 解決策
770件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @batch202563,

Could you share which RTD package and product you are using? Also, are you creating an example from scratch and modifying the toolchain settings, or is does this happen with example projects as well?

I can compile projects correctly in S32DS v3.6.2, however, this seems to be an old issue with eclipse:

If it’s working, this is a known bug due the Eclipse indexer synchronization. If you delete the errors or relaunch Eclipse, it should not appear, the error message should not appear.

Best regards,
Julián

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
771件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @batch202563,

Could you share which RTD package and product you are using? Also, are you creating an example from scratch and modifying the toolchain settings, or is does this happen with example projects as well?

I can compile projects correctly in S32DS v3.6.2, however, this seems to be an old issue with eclipse:

If it’s working, this is a known bug due the Eclipse indexer synchronization. If you delete the errors or relaunch Eclipse, it should not appear, the error message should not appear.

Best regards,
Julián

0 件の賞賛
返信
752件の閲覧回数
batch202563
Contributor I

Thank you for your answer.
I got an error when I imported a project created in V3.5.
I'll study more using the example projects and then ask a question.

0 件の賞賛
返信