Hi,
I'm trying to examine the CAN-FD robustness and operation using the S32K Freedom boards and using the design studio.
While other examples can be compiled and ran in the boards freely, the CAN-FD Master/Slave do compile but I get an Error when I try to run/debug it.
When I try to Run as S32DS C/C++ Application (with Debug_RAM or Debug_FLASH) I get:
When I try to Debug as S32DS C/C++ Application with GDB (Debug_RAM or Debug_FLASH) I get:
I installed GDB on my windows but not sure how to connect it to the project.
When I try to Debug as S32DS C/C++ Application with JLINK (Debug_RAM or Debug_FLASH) I get:
I would appreciate any assistance.
Best regards,
Ilan Sharon
Hello IIan,
Which version of S32DS are you using?
I'd recommend you to download the latest release:S32 Design Studio for ARM v1.3 (Windows/Linux) released!
According to the screenshots this seem like a debug configuration issue.
1) Do not use menu "Run" to load the project: MPC5744P running problem use "Debug" instead
2) make sure your P&E/ Segger GDB debug configuration is correct and complete:
e.g. Segger configuration seems to have wrong -device PKE18F... set (I assume you are targeting S32K144)
I'd recommend you to create a dummy project and compare its debug configuration with an example one.
P&E GDB error message indicates there might be missing some information in debug configuration please check highlighted fields:
Hope it helps.
Stan
Hi Stan,
Thank you for returning to me.
Problem was already solved.
Best regards,
———————————————————
Ilan Sharon
EBV Field Application Engineer
———————————————————
Office:
+972-9-7780343
Mobile:
+972-54-6385244
———————————————————
www.Avnet-Israel.co.il<http://www.avnet-israel.co.il/activities/>;
Line Card<http://www.avnet-israel.co.il/linecard/>
All of Avnet's quotes and accepted orders are subject to Avnet's Standard Terms And Conditions<http://www.avnet-israel.co.il/terms-and-conditions/> of Sale which appear on Avnet's quotations, packing slips, invoices and the website.