Hello ,
thanks for sharing your gcc source code (4.9.4).
I have tried to compile the gcc on linux version
(gdb part)
i have some errors
libtool: compile: i686-pc-mingw32-gcc -DHAVE_CONFIG_H -I. -D__USE_MINGW_FSEEK -I. -I. -I./../include -DHAVE_powerpc_elf32_vec -DHAVE_rs6000_xcoff_vec -DHAVE_powerpc_elf32_le_vec -DHAVE_powerpc_boot_vec -DHAVE_elf32_le_vec -DHAVE_elf32_be_vec -DHAVE_plugin_vec -DBINDIR=\"/opt/freescale/gcc-4.9.4-Ee200-eabivle/i686-mingw32/bin\" -W -Wall -Wstrict-prototypes -Wmissing-prototypes -Wshadow -Wno-format -Werror -g -O2 -D__USE_MINGW_ACCESS -MT coffgen.lo -MD -MP -MF .deps/coffgen.Tpo -c coffgen.c -o coffgen.ocoffgen.c: In function ‘coff_print_symbol’:coffgen.c:2118:5: error: empty declaration [-Werror] __attribute__ ((fallthrough)); ^coffgen.c:2139:5: error: empty declaration [-Werror] __attribute__ ((fallthrough)); ^
do we need the last version of gcc to compile or not ?
Best regards
Erwan
已解决! 转到解答。
Yes
Remove this line from list of pathes in "f-sources/F494"
gdb.7-8-2_fix-fallthrough \
在原帖中查看解决方案
What Linux host do you use for build ?
At least ib tuilts on Ubuntu 16 and Fedora 22
Hello Alexander ,
I am using Ubuntu 14.04.5 LTS linux kernel 3.13.0-71-generic x86_64
i think that this following attribute only for gcc7
__attribute__((fallthrough));
Maybe , you have used gcc7 to compile powerpc-vle-gcc-4.9.4 ?