PWM generation using FLEX timers other FTM0 for s32k144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PWM generation using FLEX timers other FTM0 for s32k144

1,545 次查看
sayali_ayarkar
Contributor I

Hi,

I have used PWM generation example for s32k144. In that example, FTM0 , channel 0 is used which works fine.

I tried changing channels and it works.

But when I  try to change FTM0 to FTM1/2/3. I am not able to see PWM generation.

Is there any restrictions for PWM generation using FTM? Is it only possible using FTM0?

Do we have to do some settings for PWM generation using other FTM?

P.S. I am using Processor expert code generation.

Thanks

0 项奖励
回复
1 回复

1,476 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sayali,

If you can attach the project here, we can help you faster.
Or "PrtScn" the setting of Processor Expert and "paste" here.

How do you see the PWM? Use an oscilloscope to measure waveform on the S32K144EVB pins or direct see the light of RGB_LED?

Notice the difference between different FTM module.

FTM S32K144.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复