PLS Support on S32 Design Studio for Power Architecture v1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PLS Support on S32 Design Studio for Power Architecture v1.1

3,012 次查看
wan35fr
Contributor III


Hello ,

 

on version 1.1, i did not find PLS support on the project Wizard on MPC5601D

Did you support this debugger ?

 

154420_154420.png2016-06-28_113650.png

 

       Best regards

 

                      Erwan

0 项奖励
回复
5 回复数

2,647 次查看
stanish
NXP Employee
NXP Employee

Hello Erwan,

The PLS debugger Eclipse Plugin is not installed by default in s32DS.

It's necessary to download it from pls-mc.com and install first. Once it's installed it should appear on the Debugger list  in project wizard.

I'm preparing step-by-step instructions. I'll post it on community as soon as it's ready.

Regards,

Stan

0 项奖励
回复

2,647 次查看
xuantruongdao
NXP Employee
NXP Employee

Hello Stan,

I see if want  to have plugin PLS for Eclipse, have to install PLS software. Could you tell me how i can  download Plugin only, I try to find in pls-mc.com but cannot.

Thank you so much.

0 项奖励
回复

2,647 次查看
wan35fr
Contributor III

Hello Xuan ,

1) you can download  PLS UDE Engine from http://www.pls-mc.com

2016-08-10_101053.png

2) The PLS eclipse plugins should be installed in Program Files/UDE directory

3) Use Install New Software (Eclipse) to install a local update site in S32 Design Studio

    Best regards

                      Erwan

0 项奖励
回复

2,647 次查看
xuantruongdao
NXP Employee
NXP Employee

Hello Erwan,

Thank you so much, I did but cannot, may be my account is not be allowed.

PLS1.png

I ask support team long time ago:

PLS_ASK.png

I don't have any hardware PLS as well as purchased UDE version. I need plugin only.

you  said you can debug and flash but I see a error in debug configuration - I think due to plugin or UDE not be installed in my machine.

PLS_Debug.png

Best Regards,

Truong

0 项奖励
回复

2,647 次查看
wan35fr
Contributor III

Hello Stan ,

it is working well with Luna Eclipse Plugins from PLS ;-)

i can flash and debug with PLS from S32 Design Studio.

          Best Regards

                                 Erwan

0 项奖励
回复