PEMicro not shown in "Run configuraiton..."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEMicro not shown in "Run configuraiton..."

Jump to solution
577 Views
LeoZ
Contributor III

In S32 Design Studio, "PEMicro" only show in "Debug Configurations" but not show in "Run Configurations"

How could I add "PEMicro" to "Run Configurations". Because I often just want to download code to board to run with the "Run" button, not need to debug

noe_1.jpg

Labels (1)
0 Kudos
1 Solution
562 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

for embedded systems there is no reason for using Run configurations. You always need to use debug probe (except the systems with OS which can execute gdb server). Please use Debug Configurations.  

View solution in original post

0 Kudos
2 Replies
563 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

for embedded systems there is no reason for using Run configurations. You always need to use debug probe (except the systems with OS which can execute gdb server). Please use Debug Configurations.  

0 Kudos
543 Views
LeoZ
Contributor III

Got it,and I am going to use debug. Actually, I use the "Run" to work as a "download" button for programming code to board without "debug" (no "download" button in S32 Design Studio).

0 Kudos