PEMicro does not show on "S32DS Extensions and Updates"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEMicro does not show on "S32DS Extensions and Updates"

Jump to solution
1,368 Views
GaryZhang1
Contributor III

I have installed "S32DS.3.5_b220726_win32.x86_64.exe" with "SW32K3xx.S32DS_3.5.0_D2212.zip", I saw PEMicro installed and see "C:\PEMicro\PEDrivers" but I do not see it in "S32DS Extensions and Updates", is it a problem?

Thanks

Gary

0 Kudos
Reply
1 Solution
1,336 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @GaryZhang1 , 

Are you able to see the option from the "Install new software"

Mehul_Patel_NXP_0-1690309871785.png

 

View solution in original post

0 Kudos
Reply
3 Replies
1,331 Views
GaryZhang1
Contributor III

Hi @Mehul_Patel_NXP

Yes, I am ok to open "Install new software". I am able to see PEMicro now after re-installation, so I no longer have the question. thanks.

0 Kudos
Reply
1,299 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Great! Thank you for your reply. 

0 Kudos
Reply
1,337 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @GaryZhang1 , 

Are you able to see the option from the "Install new software"

Mehul_Patel_NXP_0-1690309871785.png

 

0 Kudos
Reply