Hi,
My target is S32K146 , I'm trying to partition the part. I did this successfully last night.
However when I tried to connect to S32K DESIGN STUDIO this morning I get the following after it attempts to program the part.:
"Connection closed by the GDB server".
and it fails. The part is unsecured.
I don't see this happening with the other projects.
what could cause this to happen?
Best Regards,
Koorosh Hajiani
Hi Jiri:
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "57101" to 6224
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "57102" to 7224
Telnet server running on 127.0.0.1:51794
Searching for FreeRTOS Kernel Symbols...
rsp_qC - qSymbol: 707843757272656E74544342
pxCurrentTCB not found. FreeRTOS analysis not enabled.
Copyright 2018 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS_ARM_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne.expansion_4.3.5.201910081615\win32\pegdbserver_console -device=NXP_S32K1xx_S32K146F1M0M11 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -s€
CMD>RE
Initializing.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_ARM_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne.expansion_4.3.5.201910081615\win32\gdi\P&E\supportFiles_ARM\NXP\S32K1xx\freescale_s32k146f1m0m11_pflash_dflash_eeprom.arp
Initializing.
Initialized.
;version 1.03, 11/30/2017, Copyright 2017 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [s32k146f1m0m11_x_pflash_dflash_eeprom]
;device freescale, s32k146f1m0m11, pflash_dflash_eeprom
;begin_cs device=$00000000, length=$14001000, ram=$20000000
Loading programming algorithm ...
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00000000-00000043 ...
Ok.
block 0000040C-0000040F ...
Ok.
block 00000500-0000FF05 ...
Ok.
block 0000FF08-00016523 ...
Ok.
block 0001FFF0-0001FFFF ...
Ok.
block 00060300-000FFFFF ...
Ok.
block 10000000-1000FFFF ...
Error! CRC Command Timed Out
Current content of flash does not match application to be programmed
CMD>EM
Command is inactive for this .ARP file.
Error Erasing flash of device
Error occured during Flash programming.
PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.
Thanks,