Only CAN_0 in S32DS Debug view

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Only CAN_0 in S32DS Debug view

1,774 Views
bdn
Contributor III

Hi,

 

why is there only CAN_0 in S32_Debug view as seen on the screenshot?

153614_153614.pngCAN.png

 

I'm using S32DS for PowerPC in verison 1.0 with MPC5748G Eval Board and 176QFP Daughtercard.

 

Regards,

Bernhard

Labels (2)
2 Replies

1,564 Views
bdn
Contributor III

Hi,

this issue is _not_ fixed in S32 DS for Power Architecture 1.1.

Regards

1,564 Views
martin_kovar
NXP Employee
NXP Employee

Hi Bernhard,

I checked the issue and you are correct, there is only CAN_0. It seems it is a bug, so I reported it immediately. Sorry for inconvenience, I hope it will be fix in the next release, which should be available at the end of June.

As a workaround, memory view could be used.

Regards,

Martin

0 Kudos
Reply