Multiple timers configuration on S32K1xx by S32DS SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple timers configuration on S32K1xx by S32DS SDK

ソリューションへジャンプ
1,747件の閲覧回数
wei_w_he
Contributor IV

Dear Officer,

We are using S32DS with SDK for development Motor control with hall sensor project.on S32K118.

When configure the ic_pal module via Component then auto-generate code, I notice can't configure 2 timer channel with same FTM device. e.g.after configure FTM0 CH0 (PTC0) by ic_pal1, then can't configure ic_pal2 to use FTM0 CH1 (PTC1) because it mention FTM0 is taken by ic_pal1.

How to configure and auto-generate code for 2 timers with same FTM device? One FTM device can support upto 8 timer channels simultaneously?

Thanks and best regards

He Wei

0 件の賞賛
返信
1 解決策
1,744件の閲覧回数
wei_w_he
Contributor IV

It is resolved. pls ignore it.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,745件の閲覧回数
wei_w_he
Contributor IV

It is resolved. pls ignore it.

0 件の賞賛
返信