Dear Officer,
We are using S32DS with SDK for development Motor control with hall sensor project.on S32K118.
When configure the ic_pal module via Component then auto-generate code, I notice can't configure 2 timer channel with same FTM device. e.g.after configure FTM0 CH0 (PTC0) by ic_pal1, then can't configure ic_pal2 to use FTM0 CH1 (PTC1) because it mention FTM0 is taken by ic_pal1.
How to configure and auto-generate code for 2 timers with same FTM device? One FTM device can support upto 8 timer channels simultaneously?
Thanks and best regards
He Wei
Solved! Go to Solution.
It is resolved. pls ignore it.