Multiple timers configuration on S32K1xx by S32DS SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple timers configuration on S32K1xx by S32DS SDK

Jump to solution
1,697 Views
wei_w_he
Contributor IV

Dear Officer,

We are using S32DS with SDK for development Motor control with hall sensor project.on S32K118.

When configure the ic_pal module via Component then auto-generate code, I notice can't configure 2 timer channel with same FTM device. e.g.after configure FTM0 CH0 (PTC0) by ic_pal1, then can't configure ic_pal2 to use FTM0 CH1 (PTC1) because it mention FTM0 is taken by ic_pal1.

How to configure and auto-generate code for 2 timers with same FTM device? One FTM device can support upto 8 timer channels simultaneously?

Thanks and best regards

He Wei

0 Kudos
Reply
1 Solution
1,694 Views
wei_w_he
Contributor IV

It is resolved. pls ignore it.

View solution in original post

0 Kudos
Reply
1 Reply
1,695 Views
wei_w_he
Contributor IV

It is resolved. pls ignore it.

0 Kudos
Reply