Multiple timers configuration on S32K1xx by S32DS SDK

cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple timers configuration on S32K1xx by S32DS SDK

Jump to solution
102 Views
Contributor IV

Dear Officer,

We are using S32DS with SDK for development Motor control with hall sensor project.on S32K118.

When configure the ic_pal module via Component then auto-generate code, I notice can't configure 2 timer channel with same FTM device. e.g.after configure FTM0 CH0 (PTC0) by ic_pal1, then can't configure ic_pal2 to use FTM0 CH1 (PTC1) because it mention FTM0 is taken by ic_pal1.

How to configure and auto-generate code for 2 timers with same FTM device? One FTM device can support upto 8 timer channels simultaneously?

Thanks and best regards

He Wei

0 Kudos
1 Solution
99 Views
Contributor IV

It is resolved. pls ignore it.

View solution in original post

0 Kudos
1 Reply
100 Views
Contributor IV

It is resolved. pls ignore it.

View solution in original post

0 Kudos