Move S32DS3.4 license to New Computer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Move S32DS3.4 license to New Computer

Jump to solution
1,909 Views
m_c
Senior Contributor I

Hello,

My old computer was broken suddenly. And I'm trying to install S32SD3.4 in my new computer. But I encountered problem will the license.

m_c_0-1725594372985.png

 

My license details:

 License Applicable to Product(s):

  Version  Description
  3.4  S32 Design Studio for S32 Platform v.3.4

 

License Quantity:Fulfillment ID:Expiration Date:Product:Machine:Activation Code:

1
119777581
Aug 26, 2028
S32 Design Studio for S32 Platform v.3.4
3288C64F4AB78208C41AECE1A81C3C989BA229B2
E4DE-FECF-56E6-BEEC
0 Kudos
Reply
1 Solution
1,867 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Go into "My NXP Account > Apps and Services > Activate my Software > View accounts > Select S32 Design Studio for S32 Platform v3.4". Once there, select "License Keys" and the License Information should be present.

After clicking the link I sent you privately, does the Total Number of Licenses increase?

Total Number of Licenses S32DSv3.4.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,860 Views
stanish
NXP Employee
NXP Employee

Hi

this issue could be caused by blocking the online communication with the licensing/activation server. I'd suggest you to try to activate the product using offline activation.

see HOWTO: Activate S32 Design Studio - NXP Community

 

Hope it helps

Stan

0 Kudos
Reply
1,868 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Go into "My NXP Account > Apps and Services > Activate my Software > View accounts > Select S32 Design Studio for S32 Platform v3.4". Once there, select "License Keys" and the License Information should be present.

After clicking the link I sent you privately, does the Total Number of Licenses increase?

Total Number of Licenses S32DSv3.4.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,812 Views
m_c
Senior Contributor I

Hello Robin,

Total Number of Licenses of v3.4 still remains 1, but v3.5 had increased.

It is very helpful when testing some software combination for customers.

Would you please also help increase it for v3.4?

Thank you very much.

 

m_c_0-1726718441316.png

 

0 Kudos
Reply