Migrate Wizard of S32DS 3.4 cannot find any project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Migrate Wizard of S32DS 3.4 cannot find any project

Jump to solution
8,318 Views
RickYeh777
Contributor III

I am trying to migrate application projects from S32DS for ARM and SDK3.0.0 to S32DS 3.4 and SDK4.0.1.
3 projects to migrate in S32DS 3.4, but S32DS 3.4 cannot find any project by migrate wizard.
Could anybody give a suggestion?
Thanks for any help.

0 Kudos
Reply
1 Solution
8,301 Views
mikedoidge
NXP Employee
NXP Employee

Hi Rick,

Have you tried the steps detailed in the following video:

Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

Best Regards,

Mike

View solution in original post

0 Kudos
Reply
4 Replies
8,292 Views
RickYeh777
Contributor III

Maybe this is the root cause.
I have S32SDK S32K1xx RTM 4.0.3. but not 4.0.2.
And migration filter is "Migrate:[S32K118] SDK S32K1xx[3.0.x]->[4.0.2]".
I don't have 4.0.2. and migration filter is not [3.0.x]->[4.0.3].

8,288 Views
RickYeh777
Contributor III

Dear Mike,

I have got 4.0.2 and this problem is solved.

Thanks for your help very much.

8,292 Views
RickYeh777
Contributor III

Thanks for your prompt response.
Yes, I had watched the video and hence had this try according to this video.
The first step is importing an archive project.
The second step is migrating it,  but I cannot find any project to migrate, that's the problem.

0 Kudos
Reply
8,302 Views
mikedoidge
NXP Employee
NXP Employee

Hi Rick,

Have you tried the steps detailed in the following video:

Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

Best Regards,

Mike

0 Kudos
Reply