Make error (msys-iconv-2.dll) in Win10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Make error (msys-iconv-2.dll) in Win10

ソリューションへジャンプ
8,240件の閲覧回数
AdrianR
NXP Employee
NXP Employee

I got a customer reporting this issue with S32DS for ARM 2.0  and 2018.R1 after Win10 installation.

No project (even clean examples) build anymore on this PC.

Could you provide guidance on how to workaround or if a Windows fix is need?

pastedImage_1.png

2 [main] make 8392 child_info_fork::abort: C:\Tool\NXP\S32DS_ARM_v2.0\utils\msys32\usr\bin\msys-iconv-2.dll: Loaded to different address: parent(0x2E60000) != child(0x26D0000)

make: fork: Resource temporarily unavailable

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
7,474件の閲覧回数
b48014
NXP Employee
NXP Employee

Hi Adrian,

You can try rebooting and run {S32DS PATH}/utils/msys32/autorebase.bat

Best regards,

Dmitry

元の投稿で解決策を見る

3 返答(返信)
7,475件の閲覧回数
b48014
NXP Employee
NXP Employee

Hi Adrian,

You can try rebooting and run {S32DS PATH}/utils/msys32/autorebase.bat

Best regards,

Dmitry

6,363件の閲覧回数
cisvmierlo
NXP Employee
NXP Employee

Hi,

For me the path to this tool was a little bit different for S32DS3.4 on windows:

C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\autorebase.bat

Kind regards,

Cis

0 件の賞賛
返信
7,474件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Adrian, 

here is similar bug - child_info_fork::abort: dll loaded to different address · Issue #477 · babun/babun · GitHub  

The Windows update should help. 

Jiri

0 件の賞賛
返信