Make error (msys-iconv-2.dll) in Win10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Make error (msys-iconv-2.dll) in Win10

Jump to solution
6,699 Views
AdrianR
NXP Employee
NXP Employee

I got a customer reporting this issue with S32DS for ARM 2.0  and 2018.R1 after Win10 installation.

No project (even clean examples) build anymore on this PC.

Could you provide guidance on how to workaround or if a Windows fix is need?

pastedImage_1.png

2 [main] make 8392 child_info_fork::abort: C:\Tool\NXP\S32DS_ARM_v2.0\utils\msys32\usr\bin\msys-iconv-2.dll: Loaded to different address: parent(0x2E60000) != child(0x26D0000)

make: fork: Resource temporarily unavailable

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
5,933 Views
b48014
NXP Employee
NXP Employee

Hi Adrian,

You can try rebooting and run {S32DS PATH}/utils/msys32/autorebase.bat

Best regards,

Dmitry

View solution in original post

3 Replies
5,934 Views
b48014
NXP Employee
NXP Employee

Hi Adrian,

You can try rebooting and run {S32DS PATH}/utils/msys32/autorebase.bat

Best regards,

Dmitry

4,822 Views
cisvmierlo
NXP Employee
NXP Employee

Hi,

For me the path to this tool was a little bit different for S32DS3.4 on windows:

C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\autorebase.bat

Kind regards,

Cis

0 Kudos
Reply
5,933 Views
jiri_kral
NXP Employee
NXP Employee

Hi Adrian, 

here is similar bug - child_info_fork::abort: dll loaded to different address · Issue #477 · babun/babun · GitHub  

The Windows update should help. 

Jiri

0 Kudos
Reply