MPC5748G: S32 software debug can not write in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G: S32 software debug can not write in

2,487件の閲覧回数
he_zhang
Contributor I

IMG_20191106_184949.jpg

Loading programming algorithm . . .

WARNING - Selected .PCP file has been modified. CRC16 = $5A63

Done.

Programming sequency is : erase, blank check, program, and verify { default }

CMD>VC

Verifying object file CRC-16 to device ranges . . .

      block 00F90000-00F9001B  . . .

 

 

When using software debug debugging, the code is written, the card is 99%, the above is the log, it seems that the chip can not be erased? Is the sector damaged?

After I replaced the MPC5748G chip, I can debug it. . .

0 件の賞賛
返信
3 返答(返信)

2,341件の閲覧回数
he_zhang
Contributor I

Yes! Can you guess the cause of this problem? Or can you provide a direction for the investigation?

thank you very much!

0 件の賞賛
返信

2,341件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

Well, you can try to use RAM Target project and check registers or just attach to running target and try to figure out what's wrong. You can also try to update OpenSDA firmware - https://community.nxp.com/docs/DOC-340263  

Jiri

0 件の賞賛
返信

2,341件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it's hard to say what's wrong - but as you said - the issue is with chip. With other MCU it is working, correct? 

Jiri 

0 件の賞賛
返信