Hi Support Team,
We recently purchased MPC5748G Rev D hardware development board. When we try to flash the examples (like Blinking LED/Flexcan program) the software is getting flashed but the when try to launch the debugging configuration we are getting the "Uncensored Device" issue. PFA The snapshot concerned with the same. We checked on the J11 jumper setting & the settings are proper for External Power Supply (12V) & 3.3 V also. We checked for both External Power supply & as well as internal power supply, but its not working. We are using the PEmicro debugger as the debugging interface. We have used the correct configurations in the S32 Debugger console.
Kindly requests you to help out to resolve this issue at the earliest.
Thanks & Regards,
Padmanabha
Hi,
what is the board used? DEVKIT-MPC5748G? If so when powering board do you see D12/D13 LEDs are ON (using external supply, J11 in 1-2 position)? For USB powering also D14 is ON (J11 in 2-3 position).
When connecting PEmicro debugger into JTAG connector, do you place it properly? Is both LEDs on debugger ON? If USB cable is connected to J1 you can try debug through OpenSDA, as showed e.g in https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP... at step 34 or in getting started guide https://www.nxp.com/document/guide/get-started-with-the-devkit-mpc5748g:NGS-DEVKIT-MPC5748G. Is the device selected in Port option of the Debug configuration? e.g. like
BR, Petr