MPC5744P running problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P running problem

1,755件の閲覧回数
hrvojeerjavec
Contributor III

I have a problem running a new S32DS project on my MPC5744P board via Multilink Universal/JTAG. It builds correctly but when I try to run the application I get "Cannot run program" error.

148793_148793.PNGCapture.PNG

It could be that my run configurations are not set right. Can anybody tell me how to set them?

 

148801_148801.PNGCapture2.PNG

ラベル(1)
2 返答(返信)

1,368件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

did you execute your program using Debug icon or Run icon? There is some issue with Run icon, which will be fixed in next release. Now please use Debug icon. If this does not help, please look at the following thread

S32DS connect PE Multilink

Regards,

Martin

1,368件の閲覧回数
hrvojeerjavec
Contributor III

This explains the source of the problem, thank you. I managed to load the code to the board through debug.