MPC5744P:"New"--"S32DS for Application Project".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P:"New"--"S32DS for Application Project".

1,482 Views
海亭刘
Contributor I

Hello all,

    MPC5744P,S32 Design Studio for Power Architecture Version 2.1.

   I did this: "File"--"New"--"S32DS for Application Project". 

   the results were as follows:

  pastedImage_1.png

Now, I want to know:Why "Cpu:MPC5744P_257"? Not  "Cpu:MPC5744P_144"

I can't to choose.

I will use "MPC5744P_144", not  "Cpu:MPC5744P_257".

 

Please , Thanks!

Tags (2)
0 Kudos
Reply
5 Replies

1,365 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

here's the procedure:

Right click on MPC5744P_257 and select Configuration Inspector:

pastedImage_1.png

Double click on MPC5744P:

pastedImage_2.png

And select version you want:

pastedImage_1.png

Then there will be a notification about problem in pin mux - just click on Switch Configuration:

pastedImage_4.png

Regards,

Lukas

0 Kudos
Reply

1,365 Views
海亭刘
Contributor I

无标题.png

hi,

Thanks for your help.

Now, I have new problems.

In the picture:

what is the different between"Debug"and"Debug_FLASH"?

why I build the "CCCCCCCCC"project, result:syntax error.

thank you!

0 Kudos
Reply

1,365 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

Debug_RAM can be used to development purposes - the project is loaded to RAM, not to flash. It's faster because flash programming is not necessary. RAM size is a limitation, of course. When the project size grows up, you can switch to Debug_Flash.

Was the project "CCCCCCCCC" created in this version of S32DS or was it imported from some older version? I guess that this could be the reason.

Regards,

Lukas

0 Kudos
Reply

1,365 Views
海亭刘
Contributor I

Hi:

   I want an flexcan example project.

   I want to use ISR for flexcan recive(MB).

   pastedImage_1.png

pastedImage_2.png

but ,the "CAN_IRQ" can not run.

pastedImage_3.png

thanks!

0 Kudos
Reply

1,365 Views
海亭刘
Contributor I

HI:

  thank you for your help. the problem of the project "CCCCCCCCC" ,because the configure of our PC . NOW, it's OK.

0 Kudos
Reply