Hi,
I have a custom board made from the devkit MPC5748G. Instead of RMII, we use MII and its directly connected to another chip that uses RvMII.
Is there already some sample code available so that I can use the MII code to interact with the other chip.
Or can I reuse the ENET sample code by just changing the pin muxes and the code to
ethernet1_InitConfig0.miiMode = ENET_MII_MODE;
Any help is appreciated.
Thanks and Regards,
Tiju
已解决! 转到解答。
Ok, I've made up an ICMP packet and with reply which toggles the led.
Here is the code.
uint8_t my_ping_data[] = {
0x18,0xdb,0xf2,0x3b,0xc0,0x59,0x11,0x22,0x33,0x44,0x55,0x66,0x08,0x00,0x45,0x00,
0x00,0x3c,0x3a,0x2c,0x00,0x00,0x80,0x01,0x7d,0x2d,0xc0,0xa8,0x01,0x12,0xc0,0xa8,
0x01,0x05,0x08,0x00,0xcd,0x8f,0x00,0x01,0x7f,0xcb,0x61,0x62,0x63,0x64,0x65,0x66,
0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,0x70,0x71,0x72,0x73,0x74,0x75,0x76,
0x77,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69
};
uint16_t length;
void build_ping(uint8_t *data)
{
#if 1
uint8_t dst_mac[6] = { 0x18, 0xdb, 0xf2, 0x3b, 0xc0, 0x59 }; /* MAC address of target */
uint8_t dst_ip[4] = { 0xc0, 0xa8, 0x01, 0x05 }; /* 192.168.1.5 IP of target */
#else
uint8_t dst_mac[6] = { 0x11, 0x22, 0x33, 0x44, 0x55, 0x66 }; /* MAC address of board */
uint8_t dst_ip[4] = { 0xc0, 0xa8, 0x01, 0x12 }; /* 192.168.1.18 IP of board */
#endif
uint8_t src_mac[6] = { 0x11, 0x22, 0x33, 0x44, 0x55, 0x66 }; /* MAC address of board */
uint8_t src_ip[4] = { 0xc0, 0xa8, 0x01, 0x12 }; /* 192.168.1.18 IP of board */
/* MAC and IP addresses */
copy_buff(&data[FRAME_ETH_DEST_MAC_OFFSET], dst_mac, 6);
copy_buff(&data[FRAME_ETH_SRC_MAC_OFFSET], src_mac, 6);
copy_buff(&data[FRAME_IP_DEST_OFFSET], dst_ip, 4);
copy_buff(&data[FRAME_IP_SRC_OFFSET], src_ip, 4);
/* Clear IP and ICMP checksums (to be filled in by the MAC) */
data[FRAME_IP_CHECKSUM_OFFSET] = 0;
data[FRAME_IP_CHECKSUM_OFFSET + 1] = 0;
data[FRAME_ICMP_CHECKSUM_OFFSET] = 0;
data[FRAME_ICMP_CHECKSUM_OFFSET + 1] = 0;
/* Update ICMP type to represent Ping */
data[FRAME_ICMP_TYPE_OFFSET] = FRAME_ICMP_TYPE_ECHO_REQUEST;
}
Add this to rx_callback
else if (buffList[0].data[FRAME_IP_PROTO_OFFSET] == FRAME_IP_PROTO_ICMP &&
buffList[0].data[FRAME_ICMP_TYPE_OFFSET] == FRAME_ICMP_TYPE_ECHO_REPLY){
/* Toggle output value LED1 if we get ping reply*/
SIUL2->GPDO[LED/4] = SIUL2->GPDO[LED/4] ^ (SIUL2_GPDO_PDO_4n_WIDTH << (SIUL2_GPDO_PDO_4n_SHIFT - (8 * (LED & 0x03))));
}
In main add this:
enet_buffer_t buff;
buff.data = my_ping_data;
buff.length = sizeof(my_ping_data);
build_ping(buff.data);
for (;;)
{
/* Send back an ICMP echo reply frame */
ENET_DRV_SendFrame(INST_ETHERNET1, &buff, 1);
/* Insert a small delay to make the blinking visible */
delay(720000);
}
Thanks and Regards,
Tiju
Ok, I've made up an ICMP packet and with reply which toggles the led.
Here is the code.
uint8_t my_ping_data[] = {
0x18,0xdb,0xf2,0x3b,0xc0,0x59,0x11,0x22,0x33,0x44,0x55,0x66,0x08,0x00,0x45,0x00,
0x00,0x3c,0x3a,0x2c,0x00,0x00,0x80,0x01,0x7d,0x2d,0xc0,0xa8,0x01,0x12,0xc0,0xa8,
0x01,0x05,0x08,0x00,0xcd,0x8f,0x00,0x01,0x7f,0xcb,0x61,0x62,0x63,0x64,0x65,0x66,
0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,0x70,0x71,0x72,0x73,0x74,0x75,0x76,
0x77,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69
};
uint16_t length;
void build_ping(uint8_t *data)
{
#if 1
uint8_t dst_mac[6] = { 0x18, 0xdb, 0xf2, 0x3b, 0xc0, 0x59 }; /* MAC address of target */
uint8_t dst_ip[4] = { 0xc0, 0xa8, 0x01, 0x05 }; /* 192.168.1.5 IP of target */
#else
uint8_t dst_mac[6] = { 0x11, 0x22, 0x33, 0x44, 0x55, 0x66 }; /* MAC address of board */
uint8_t dst_ip[4] = { 0xc0, 0xa8, 0x01, 0x12 }; /* 192.168.1.18 IP of board */
#endif
uint8_t src_mac[6] = { 0x11, 0x22, 0x33, 0x44, 0x55, 0x66 }; /* MAC address of board */
uint8_t src_ip[4] = { 0xc0, 0xa8, 0x01, 0x12 }; /* 192.168.1.18 IP of board */
/* MAC and IP addresses */
copy_buff(&data[FRAME_ETH_DEST_MAC_OFFSET], dst_mac, 6);
copy_buff(&data[FRAME_ETH_SRC_MAC_OFFSET], src_mac, 6);
copy_buff(&data[FRAME_IP_DEST_OFFSET], dst_ip, 4);
copy_buff(&data[FRAME_IP_SRC_OFFSET], src_ip, 4);
/* Clear IP and ICMP checksums (to be filled in by the MAC) */
data[FRAME_IP_CHECKSUM_OFFSET] = 0;
data[FRAME_IP_CHECKSUM_OFFSET + 1] = 0;
data[FRAME_ICMP_CHECKSUM_OFFSET] = 0;
data[FRAME_ICMP_CHECKSUM_OFFSET + 1] = 0;
/* Update ICMP type to represent Ping */
data[FRAME_ICMP_TYPE_OFFSET] = FRAME_ICMP_TYPE_ECHO_REQUEST;
}
Add this to rx_callback
else if (buffList[0].data[FRAME_IP_PROTO_OFFSET] == FRAME_IP_PROTO_ICMP &&
buffList[0].data[FRAME_ICMP_TYPE_OFFSET] == FRAME_ICMP_TYPE_ECHO_REPLY){
/* Toggle output value LED1 if we get ping reply*/
SIUL2->GPDO[LED/4] = SIUL2->GPDO[LED/4] ^ (SIUL2_GPDO_PDO_4n_WIDTH << (SIUL2_GPDO_PDO_4n_SHIFT - (8 * (LED & 0x03))));
}
In main add this:
enet_buffer_t buff;
buff.data = my_ping_data;
buff.length = sizeof(my_ping_data);
build_ping(buff.data);
for (;;)
{
/* Send back an ICMP echo reply frame */
ENET_DRV_SendFrame(INST_ETHERNET1, &buff, 1);
/* Insert a small delay to make the blinking visible */
delay(720000);
}
Thanks and Regards,
Tiju
Hello Tiju,
The sample code should work with the changes mentioned by you: updating the pins configuration and the miiMode field of the ENET driver configuration structure.
Please let me know if you have any issues.
Best regards,
Veronica
Hi Veronica,
Thanks for confirming.
Is there a sample transmit code (ICMP) for ENET available to test by enabling the loopback in the code available by default?
If not, how can we test the interface?
Thanks and Regards,
Tiju