MCAL Gpt Driver Api error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAL Gpt Driver Api error

ソリューションへジャンプ
756件の閲覧回数
jwjung
Contributor II

hi,

 

i tried to use MCAL Gpt driver but i can't call the Api.

 

like below,

jwjung_0-1755157473685.png

 

i setup the parameter to use the Api but i can't pass the line (#if )

 

how can i solve this problem.

 

thanks,

 

attachment

chip : NXP S32K312

RTD : SW32K3_RTD4.4_R11-21_3.0.0_DS2303

DS : S32 Design Studio for S32 Platform, Version: 3.5

 

and review the gpt_example but the problem is remain.

 

0 件の賞賛
返信
1 解決策
741件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jwjung 

This issue usually occurs due to unresolved index references in the project.

To resolve it, right-click on the project name in the Project Explorer, then go to Index > Rebuild. This will force Eclipse to re-index the project and should help clear up the issue.

 

BR, VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
742件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jwjung 

This issue usually occurs due to unresolved index references in the project.

To resolve it, right-click on the project name in the Project Explorer, then go to Index > Rebuild. This will force Eclipse to re-index the project and should help clear up the issue.

 

BR, VaneB

0 件の賞賛
返信